Skip to main content

UTC Fire & Security DK Adds New Control Panels to Popular Systems Line

UTC Fire & Security DK A/S has extended its popular Advisor™ Advanced intrusion systems line with the launch of three new control panels offering a range of high-end features,  including easy mobile connectivity through the UltraSync™ remote management mobile application. UTC Fire & Security DK A/S is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

The new ATS1500A, ATS3500A and ATS4500A control panels improve commissioning and remote servicing and allow for future system upgrades. For example, the intrusion control panels come with the option to expand to cloud-based solutions. Compatible with both the UltraSync IP platform and the ATS8600 security management system, the new intrusion control panels offer users a wide range of options for remote monitoring and site control. They are also compatible with the latest detectors and intrusion devices.

The panels are ideal for new installations ranging from 32 detectors up to 512. With legacy systems, users can upgrade but retain all of their existing cabling and detectors. In addition, a user-friendly installation wizard makes it easy to install the settings for Grade 2 and Grade 3 systems.

“Upgrading to the latest Advisor Advanced technology gives users the flexibility of using a mobile app to control their system,” explains Frank Thillerup, pre-sales engineer, UTC Fire & Security DK A/S. “Users can set and disable the system and perform a range of diagnostic and control tasks using a tablet or phone.”

The new panels can be used with the latest generation of intrusion devices, such as Aritech® wireless PIRcam sensor, a flexible wireless security solution.

“The system accessibility allows system designers and installers to improve the performance of legacy systems, or to design new systems with the most advanced, high-security features and area hierarchies,” added Thillerup.

The new Advisor Advanced panels are all available in IP and non-IP formats. Full training and free support is provided in Denmark for all UTC Fire & Security products.

For more information, visit www.utcfssecurityproducts.dk.

About UTC Climate, Controls & Security
UTC Climate, Controls & Security is a leading provider of heating, ventilating, air conditioning and refrigeration systems, building controls and automation, and fire and security systems leading to safer, smarter, sustainable and high-performance buildings. UTC Climate, Controls & Security is a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.ccs.utc.com or follow @UTC_CCS on Twitter.